Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Download Service fails to start after an upgrade to v.4.2.251

Warning

 

Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support for assistance.

Issue

Download Service fails to start after an upgrade to v.4.2.251

Product Line

  • Security Expert

Environment

  • Security Expert Server v4.2.251

Cause

Miscrosoft Visual C++ 2013 Redistributible  (VC++ 2013 Redist v120) is not installed. This package is a pre-requisite to installing Security Expert v4.2.251.

Resolution

Locate the file on the Microsoft site https://www.microsoft.com/en-nz/download/details.aspx?id=40784. Download and install the 32 bit version (because Security Expert is a 32 bit application) before performing the upgrade.  

Labels (1)
No ratings
Version history
Revision #:
5 of 5
Last update:
2 weeks ago
Updated by:
 
Contributors