Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to call pILiveData error when editing Schedule object in Continuum 1.94.

Issue

After upgrading to Continuum 1.94, Cyberstation throws the following error. 

Failed to call pILiveData -> GetLiveData().  ACDataServices has an error.

Environment

Continuum 1.94

Schedule

Error

Cause

This behaviour is due to a bug that was described in TPA-BOST-12-0002 00 Schedule Exception Errors.

Resolution

Install the CyberStation v1.94 SP1 - Software which can be found on the Exchange Extranet.

Tags (1)
Labels (1)
Version history
Revision #:
4 of 4
Last update:
a week ago
Updated by:
 
Contributors