Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Folders have disappeared from navigation pane in folder explorer

Issue

With revision 1.0.37 and later, folders under the instance within the navigation tree are no longer there.

 

2018-10-29_9-35-57.jpg

Product Line

Access Expert

Environment

  • V3 Hosted

Cause

The 1.0.37 release of the Keep software removed the folders under the instance within Folder Explorer.

Resolution

Use the corresponding tabs at the top of the window.

2018-11-26_9-48-39.jpg

 

Labels (1)
No ratings
Version history
Revision #:
5 of 5
Last update:
‎2018-11-26 07:50 AM
Updated by: