Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

HID Corporate 1000 support in Security Expert

Issue

What HID Corporate 1000 card formats are supported by Security Expert? 

Product Line

 Security Expert

Environment

  • Security Expert Server
  • Security Expert Controller
  • Security Expert Smart Card Reader 

Cause

Information about HID Corporate 1000 card formats is needed to configure the card readers correctly. The existing documentation does not mention this.

Resolution

Some Corporate 1000 formats have been validated and may work using the provided Reader 1 Format setting which uses a 35-bit format. It is located in the drop-down menu Expanders > Reader Expanders > Reader x as shown below. Other formats may work however it is recommended to first test these cards.  

reader formats.jpg
If the format specification is known, it is possible to program the cards as a custom format.
If not known, Product Support will need RAW card reads from at least 3 different cards for each bit length, i.e. 3 cards where the length is 36 bit and 3 cards where the length is 42 bits.

This can be gathered by navigating to Expanders > Reader Expanders and setting the Reader Format to Any Bit RAW, then badging your cards. When this is done take screenshots of the reader events by executing an Event Search or create an Event Filter for All Reader Events.

event search.jpg

Refer to KB article Show raw card data of a badged card in Security Expert for further details.

Labels (1)
No ratings
Version history
Revision #:
9 of 9
Last update:
‎2018-12-14 01:43 AM
Updated by:
 
Contributors