Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Linux information on the Automation Server

Issue

Information concerning Linux releases used within the Automation Server.  

Product Line

EcoStruxure Building Operation

Environment

  • Linux Operating System (OS)
  • Building Operation Automation Server
  • Building Operation Automation Server Premium

Cause

Questions concerning Linux releases used within the Automation Server.

Resolution

AS versions to 1.4.1 run Linux kernel 2.6.25.1
AS versions 1.5 to 2.0.2 run Linux kernel 3.0.101
AS-P versions 1.7 to 2.0.2 run Linux kernel 3.5.0-lsp-3.3.1

For questions concerning what type of Linux...i.e. Red Hat, Ubuntu, openSUSE - There is no linux distribution in the automation server just vanilla linux kernel. For further reading, download some documentation about the kernel from their website www.kernel.org


 

Labels (1)
No ratings
Version history
Revision #:
3 of 3
Last update:
‎2018-11-26 06:57 PM
Updated by:
 
Contributors