Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Pin-pad reader bit formats supported with Security Expert Controller (SP-C)

Issue

What bit formats are accepted by the Security Expert Controller (SP-C) for communicating with third-party card reader with pin?

Product Line

Security Expert

Environment

  • Security Expert Server 4.2.x
  • Security Expert Controller (SP-C) 2.08.x

Cause

When using pin pad readers with the Security Expert Controller (SP-C) there are only a few supported bit formats. Only these current formats are support and tested with the product at this time. 

Resolution

Security Expert currently supports the following formats:

  • 26 Bit (Site 0)
  • ARK-501
  • 4 Bit
  • 4 Bit Parity
  • 4 Bit Buf
  • 4 Bit Buf & Par
  • 36 Bit (IEI S0)
Labels (1)
No ratings
Version history
Revision #:
11 of 11
Last update:
‎2018-12-14 01:30 AM
Updated by:
 
Contributors