Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

VisiSat 2.1 Build 185 the Points Gallery does not show any points.

Issue

Using special characters or certain regional characters in the VisiSat Points gallery

Environment

special characters

regional characters

VisiSat Points gallery

alt

Cause

This issue is specific to VisiSat version 2.1 Build 185.

VisiSat 2.1 older releases (Builds 14, 17,137,148 sp1) are not affected.

Example of some of the special characters available:

Ù, Ú, Û, ©, è, é, ®, ±, ¼, ½, ¾, Ò, Ó, Ô, Õ. ° (Degree “alt+248”)

Resolution

Details of the issue and some options available to you are covered in TPA-SACH-12-0005.00 - VisiSat Build 185 Pointlist issue.

Tags (1)
Labels (1)
Version history
Revision #:
2 of 2
Last update:
2 weeks ago
Updated by:
 
Contributors