Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Workstation Pro License fails to allow running of v2.0 EcoStruxure following an upgrade

Issue

Workstation Pro License fails to allow running of v2.0 EcoStruxure WorkStation following an upgrade

Product Line

EcoStruxure Building Operation

Environment

WorkStation

Cause

Workstation Pro License SXWSWWORK00002 (SW-STATION-PRO-0) is the same for v1.x and v2.x, so that WorkStation Pro should continue to operate after an upgrade.

However, there was a License upgrade/change at v1.7 (from v1 to v2) and if the License was registered before this the version remains at v1 and this will not run v2.x WorkStation

Resolution

The WorkStation Pro License needs to be returned, then re-installed using the online Licensing system.

 Licenses Marked.jpgBefore License is returned

 

 Licenses after reactivation Marked.jpgAfter license is returned

 The process to return a license can be found in Webhelp.

 

Labels (1)
100% helpful (1/1)
Version history
Revision #:
6 of 6
Last update:
‎2018-10-03 02:38 AM
Updated by:
 
Contributors